2024-07-06 01:19 PM
I have a node connected to a gateway and a chirpstack server. I decided I want to understand a few topics. So I went into the above file and changed the EUI from a working 80,00,00,00,00,00,00,06 to below.
#define LORAWAN_JOIN_EUI A0,01,B0,02,C0,03,D0,04
I rebuild code and the node still works with the network server which has listed the 80....EUI number.
I am running the node as OTAA but cannot understand why the new EUI won't take. Can someone please explain how to make this work?
2024-07-09 03:06 AM
Hello @SWenn.1
I suggest you try to disconnect and reconnect the Node with new parameters. That may do the Job.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.