cancel
Showing results for 
Search instead for 
Did you mean: 

RSSI on LoRa-E5 vs nucleo-WL55JC1

spa23
Associate III

Hi

i'm just sitting and messing with a few lora boards.

I find that nucleo-WL55JC1 has approx 10dbm RSSI better than seeed LoRa-E5, and that nucleo-WL55JC1 also transmits with a more powerful signal, what is your experience ??

with best regards

12 REPLIES 12

What do you mean exactly when you said the clock domain on one GPIO wasn't right? Which pin?

I see an issue in my application where the receiver appears to be desensed about 10 dB. I'm wondering if I have the same problem that you were seeing.

@DWalk.3 You're replying to a nearly two year old thread, and it doesn't seem that @spa23 has had any activity on the forum since then.


@DWalk.3 wrote:

I'm wondering if I have the same problem that you were seeing.


The problem stated was with an RF switch control pin - so, if you have an RF switch, check that its control pins are really in the state they should be in...

DWalk.3
Associate III

I saw that after the fact. It looks like my RF pins are correct.