2022-12-27 10:28 PM
Hello
I request more antenna specification for STM32WB5MMG.
As datasheet, already provided, there is an antenna radiation patterns and efficiency but no more information about peak gain etc.
If there is an antenna performance report, that shuld be the best.
sincerely
2023-01-02 01:05 AM
Hello @YKang.5,
You can look the AN5434 in the section 7, there are some performance parameters for the PCB printed antenna.
Kind regards,
Morgane
When your question is answered, please close this topic by choosing "Select as Best". This will help other users find that answer faster 😊
2023-01-15 08:46 PM
Thanks for your reply.
The AN5434 is about on-board antennas, including chip anatenna which is included in STM32WB5MMG.
However, it has only one paragraph and lacking performance specs.
The data I found is only 'antenna radiation patterns' in datasheet of STM32WB5MMG, and the paragraph 3.8 at AN5434.
Is there any more data that I could use?