2022-02-11 5:18 AM
We design a new product where we use STM32WL microcontroller and in the datasheet ST is recommended to use NT2016SF-32M-END5875A, it was not in stock everywhere. We planned to use the ECS-TXO-20CSMV-320-EY-TR TCXO in our design. Please share your recommendation regarding this part number. if you have any alternate part, please share.
2022-02-11 8:02 AM
The shortages tend to result from a fire at AKM rather than directly related to the wider IC capacity issue.
See Data Sheet, gives actual expectations, make a judgement, perhaps work with a FAE assigned to your account.
1.8V (but you have option to program voltage between 1.6 and 3.3V depending on supply)
max 4mA current draw
clipped sine 1.2 Vpp MAX
+/-3.6 ppm