2022-01-08 6:51 PM
I've read all topics regarding this error on the forum but nothing helped.
The borad connected to Arduino connector is USI® WM-SG-SM-42.
Projects build succesfully and connect with the board through ST-Link v3. This is the output I get when debugger and low power work is not enabled(set to 0):
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0-RC01
-------------------------------------------------------------------
ST-LINK SN : 0667FF343339415043031750
ST-LINK FW : V2J39M27
Board : NUCLEO-L073RZ
Voltage : 3.26V
SWD freq : 950 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x447
Revision ID : Rev Z
Device name : STM32L07x/L08x/L010
Flash size : 192 KBytes
Device type : MCU
Device CPU : Cortex-M0+
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a16776.srec
File : ST-LINK_GDB_server_a16776.srec
Size : 61876 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 483]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:05.730
Verifying ...
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Shutting down...
Exit.
When debugger is enabled console output is the same, without the "Target is not responding, retrying..." part. Program just falls into HAL_PWR_EnterSLEEPMode() or HAL_PWR_EnterSTOPMode() fuction depending on low_power mode configuration. It stays there forever, which isn't an expected behaviour.
Here is a debugg configuration:
I ve spend quite a lot of time trying to find the solution and I ve run out of ideas so i will be realy greatefull for help.
2023-03-16 1:34 AM
Hello!
I'd really like to know if you managed to find a solution to this problem. I'm in the same predicament as you were (still are? I hope not.).
Kind regards,
Thines
2023-03-16 4:18 AM
Hey there, I've seen this error before and only way I know is to enable the debug.
Try to find \Core\Inc\sys_conf.h header file and set the following definitions as such.
DEBUGGER_ENABLED 1
LOW_POWER_DISABLE 1
Have you tried this?