cancel
Showing results for 
Search instead for 
Did you mean: 

Product Confusion

fabltd
Associate III

Hello All

I am very confused about picking the correct STM32WL for LoRaWAN. 

There appears to be:

STM32WL5MOC - The datasheet says this is a STM32WL55JC - What does the MOC add? 

Then there is the:

STM32WL55CC

STM32WL55JC

From what I can tell is the CC has less pins. 

Then we get to buying these:

STM32WL55CC (U6) 

STM32WL55CC (U7)  

Whats the difference between U6 and U7 - This is not mentione in the datasheet

The MOC is offered as:

STM32WL5MOC (H6TR) 

STM32WL5MOC (H6STR) 

Whats the difference between H6TR  and H6STR 

For development we are considering using the:

B-WLM5-SUBG1 development board. This contains the STM32WL5MOC  not sure doesn't say H6STR or H6TR

Is there a recommed STLINK-V3  programmer to use with this series?

Thank you

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @fabltd and welcome to the ST Community.

For the STM32WL55, they are MCU (Microcontrollers). you can find all explanation about the naming on the part 7 of the datasheet:

STTwo32_0-1729865959266.png

For the STM32WL5MCO, is a module based on the STM32WL55JC that you can use it on standalone mode or connect it to a SOC with an external MCU that control it. More data are available on this datasheet.

For the B-WLM5-SUBG1 development board, it is based on the STM32WB5MMGH6TR.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7

6 / 7 relates to temperature, and IS in the datasheet

https://www.st.com/resource/en/datasheet/stm32wl55cc.pdf#page=147

 

The ST-LINK/V3 would be suitable for programming/debugging

There aren't dev boards for every package combination, most of the parts share a common die, so each is a good proxy for one another.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for the confusion RE 6 and 7

Now I just need to understand the difference between the MOC and raw MCU

 

STTwo-32
ST Employee

Hello @fabltd and welcome to the ST Community.

For the STM32WL55, they are MCU (Microcontrollers). you can find all explanation about the naming on the part 7 of the datasheet:

STTwo32_0-1729865959266.png

For the STM32WL5MCO, is a module based on the STM32WL55JC that you can use it on standalone mode or connect it to a SOC with an external MCU that control it. More data are available on this datasheet.

For the B-WLM5-SUBG1 development board, it is based on the STM32WB5MMGH6TR.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi 

For the B-WLM5-SUBG1 development board the data sheet here:

https://www.st.com/resource/en/user_manual/um3127-stm32wl5moc-connectivity-expansion-board-stmicroelectronics.pdf

Mentions a STM32WL55JC  MCU?

Did I miss somthing ? 

 

Easy, the B-WLM5-SUBG1 is based on the STM32WL5MOC Module. This module is based on the STM32WL55 MCU. That's why.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi 

 

What oes the MOC module offer over the WL55 MCU?

The module advantage is that you can connect it to another SOC as a communication module. But the MCU is mainly maid to be used to run it own application that may implement or not a Communication.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.