2022-02-10 3:45 AM
Hi everyone.
I have a problem when I try to load BLE Stack on STM32WB15. I can connected the MCU to STM32Programmer and there can recognize the cortex. At the moment to load the Stack, STM32Programmer send me the configuration about FUS and I cand read it.
But, when I push Firmware Upgrade, STM32Programmer send me the next answer:
11:54:35 : STM32CubeProgrammer API v2.9.0
12:02:36 : Time elapsed during download operation: 00:00:00.498
12:02:36 : Application is running, Please Hold on...
12:02:36 : Reconnecting...
12:02:36 : Reconnected !
12:02:40 : Reconnecting...
12:02:40 : Reconnected !
12:02:41 : StartFus activated successfully
12:02:41 : FUS_STATE_IDLE
12:02:41 : Start FUS execution finished
12:02:43 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
12:02:43 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
12:02:43 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
12:02:43 : Warning: Option Bytes are unchanged, Data won't be downloaded
12:02:43 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
12:02:43 : Memory Programming ...
12:02:43 : Opening and parsing file: 0x494_FUS_Operator.bin
12:02:43 : File : 0x494_FUS_Operator.bin
12:02:43 : Size : 8 KBytes
12:02:43 : Address : 0x08000000
12:02:43 : Erasing memory corresponding to segment 0:
12:02:43 : Erasing internal memory sectors [0 3]
12:02:43 : Download in Progress:
12:02:44 : File download complete
12:02:44 : Time elapsed during download operation: 00:00:00.391
12:02:44 : Application is running, Please Hold on...
12:02:44 : Reconnecting...
12:02:44 : Reconnected !
12:02:45 : FUS_STATE_IDLE
12:02:45 : Read FUS state command execution finished
12:02:45 : UPLOADING ...
12:02:45 : Size : 4 Bytes
12:02:45 : Address : 0x20002F10
12:02:45 : Read progress:
12:02:45 : Data read successfully
12:02:45 : Time elapsed during the read operation is: 00:00:00.001
12:02:45 : UPLOADING ...
12:02:45 : Size : 4 Bytes
12:02:45 : Address : 0x8001FFC
12:02:45 : Read progress:
12:02:45 : Data read successfully
12:02:45 : Time elapsed during the read operation is: 00:00:00.001
12:02:54 : UPLOADING ...
12:02:54 : Size : 4 Bytes
12:02:54 : Address : 0x1FFF7870
12:02:54 : Read progress:
12:02:54 : Data read successfully
12:02:54 : Time elapsed during the read operation is: 00:00:00.001
12:03:36 : Old Firmware delete ...
12:03:36 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
12:03:36 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
12:03:36 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
12:03:36 : Warning: Option Bytes are unchanged, Data won't be downloaded
12:03:36 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
12:03:36 : Memory Programming ...
12:03:36 : Opening and parsing file: 0x494_FUS_Operator.bin
12:03:36 : File : 0x494_FUS_Operator.bin
12:03:36 : Size : 8 KBytes
12:03:36 : Address : 0x08000000
12:03:36 : Erasing memory corresponding to segment 0:
12:03:36 : Erasing internal memory sectors [0 3]
12:03:36 : Download in Progress:
12:03:36 : File download complete
12:03:36 : Time elapsed during download operation: 00:00:00.407
12:03:36 : Application is running, Please Hold on...
12:03:43 : Reconnecting...
12:03:46 : failed to reconnect after reset !
12:03:46 : failed to reconnect after starting FUS operator
The problem is when STM32Programmer trying to reconnected to STM32WB15 but it fail.
Someone have the same problem with the programmer?
Thank
:)
2022-02-11 3:17 AM
This problem back out again with other Custom PCB that worked before. Now, the STM32Programmer send other error when I try to start the Wireless Stack, the message is:
This is so bad because the last version of our custom PCB was working and after "try to load the new BLE stack", it does not work.
:(
2022-02-14 2:11 AM
someone have the same problem when try to do this?
2022-03-02 8:43 AM
Hello,
You can find information about FUS and wireless stack update in this wiki page:
Please try to follow instruction of this page and I hope it will correct your problem.
Best Regards,
2023-01-12 3:06 AM
Remy, no offence, but this must be the most useless reply from a ST Employee ever.
2023-08-07 7:08 AM
I am also experiencing a similar issue to this, did you find a solution?