cancel
Showing results for 
Search instead for 
Did you mean: 

Part Number: STM32WLE55CC The GPIO sink current mentioned in the data-sheet is ±8mA; The ±8mA is a total GPIO sink or source current (or) individual GPIO current? Kindly elaborate in detail.

Rahul K V
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

±20mA per pin with ±100mA max over all pins. Additionally (per data sheet):

The GPIOs can sink or source up to ±8 mA, and sink or source up to ± 20 mA (with a relaxed VOL/VOH).

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4

STM32WLE5CC !! https://www.st.com/resource/en/datasheet/stm32wle5cc.pdf

0693W00000AMuRrQAL.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Does that mean the current sink by any I/O pin is 20mA?

TDK
Guru

±20mA per pin with ±100mA max over all pins. Additionally (per data sheet):

The GPIOs can sink or source up to ±8 mA, and sink or source up to ± 20 mA (with a relaxed VOL/VOH).

If you feel a post has answered your question, please click "Accept as Solution".

Less than 5 of them would seem to be the inference

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..