cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB stuck in sequencer

DPars.2
Associate III

I have a custom board with a STM32WB55 that is getting stuck in the sequencer and stops executing as soon as I start my code. I can't tell if it's a race condition and I don't have the ability to step through the code with a debugger. The code is basically just a slightly modified version of the Nucleo Heartbeat code example. Running stm32wb5x_BLE_Stack_full v1.11.1. Here's my main():

int main(void)
{
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
 
  /* Configure the system clock */
  SystemClock_Config();
 
  //Init_Exti();
 
  MX_IPCC_Init();
 
  MX_RTC_Init();
 
  /* Init code for STM32_WPAN */
  APPE_Init();
 
  UTIL_SEQ_Init();
 
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
 
	  UTIL_SEQ_Run( UTIL_SEQ_DEFAULT );
	  /* USER CODE END WHILE */
	  HAL_GPIO_WritePin(GPIOB, LED_RGB_G_Pin, GPIO_PIN_RESET);
	  /* USER CODE BEGIN 3 */
	  BlinkTimer++;
	  if (BlinkTimer < 40000)
	  {
	      /*Configure GPIO pin Output Level */
	      HAL_GPIO_WritePin(GPIOB, LED_GREEN1_Pin|LED_GREEN2_Pin, GPIO_PIN_RESET);
	  }
	  else
	  {
	      HAL_GPIO_WritePin(GPIOB, LED_GREEN1_Pin|LED_GREEN2_Pin, GPIO_PIN_SET);
	  }
	  if (BlinkTimer > 80000) BlinkTimer = 0;
 
  }
 
}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0