2021-04-29 7:20 AM
2021-04-30 8:36 AM
±20mA per pin with ±100mA max over all pins. Additionally (per data sheet):
The GPIOs can sink or source up to ±8 mA, and sink or source up to ± 20 mA (with a relaxed VOL/VOH).
2021-04-29 7:32 AM
STM32WLE5CC !! https://www.st.com/resource/en/datasheet/stm32wle5cc.pdf
2021-04-29 10:35 PM
Does that mean the current sink by any I/O pin is 20mA?
2021-04-30 8:36 AM
±20mA per pin with ±100mA max over all pins. Additionally (per data sheet):
The GPIOs can sink or source up to ±8 mA, and sink or source up to ± 20 mA (with a relaxed VOL/VOH).
2021-04-30 9:37 AM
Less than 5 of them would seem to be the inference