2022-05-16 09:00 AM
error: no stm32 target found
If I confirm the chip is broken, I give it up immediately.It's too torturous:face_with_tears_of_joy: .
2022-05-16 09:30 AM
Pnucleo have onboard STLINK separate USB con, hope you use it.
Version STM32Programmer ?
Setup Connect under RESET...SWD interface not DFU.
2022-05-16 09:38 AM
Thanks for your responding, I have used all these ways, But it doesn't work, so i wonder the chip is bad or good?
2022-05-18 07:00 AM
Hello,
The nSWBOOT0 option byte should be set to 1 in order to use DFU mode.
Best Regards
2022-05-19 11:05 PM
Thank you, I have used this method, but it did not work.
2022-05-19 11:19 PM
I use the methods : 'ubder reset' and dfu mode. I can't solve this problem, I don't know what to do next. My guess is that the chip STM32WB55RGV6 has gone bad, but I also have no basis.