cancel
Showing results for 
Search instead for 
Did you mean: 

P_NUCLEO_WB55(stm32wb55rgv6) Help!

Lep
Senior

error: no stm32 target found

  1. Stlink is ok ,i can download program to another board.
  2. As manual's configuration, I configure MB1355C(P_NNUCLEO_WB55), I can't enter dfu mode. But the usb dongle is ok. So i think usb driver is ok.
  3. There is a 'FAIL.TXT' . The content is 'The interface firmware FAILED to reset/halt the target MCU'. I browsed through many posts , no body can solve.
  4. When i use stm32cubeprogrammer, the error is always ' no stm32 target find'. When i refresh stlink, note' STLINK error(DEV_CONNECT_ERR).
  5. I hold reset and download, it failed. I connect boot0 to 3.3V, it failed too.I don't how to continue. Does the chip(stm32wb55rgv6) is broken?

If I confirm the chip is broken, I give it up immediately.It's too torturous:face_with_tears_of_joy: .

5 REPLIES 5
MM..1
Chief III

Pnucleo have onboard STLINK separate USB con, hope you use it.

Version STM32Programmer ?

Setup Connect under RESET...SWD interface not DFU.

Thanks for your responding, I have used all these ways, But it doesn't work, so i wonder the chip is bad or good?

Remy ISSALYS
ST Employee

Hello,

The nSWBOOT0 option byte should be set to 1 in order to use DFU mode.

Best Regards

Lep
Senior

Thank you, I have used this method, but it did not work.

I use the methods : 'ubder reset' and dfu mode. I can't solve this problem, I don't know what to do next. My guess is that the chip STM32WB55RGV6 has gone bad, but I also have no basis.