2024-12-04 11:41 AM
Greetings
I have a STM32WB55 P-Nucleo board, with the STM322B55 dongle. I am trying to flash the beacon project onto the nucleo board.
I have downloaded the STM32WB repo from the github link
I unzipped the file and selected the .project from the following route:
STM32CubeWB-master\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_Beacon\STM32CubeIDE.
I tried building the project but errors are thrown that entails the file stm32wbxx.h is missing. How can I solve this?
Thanks
Solved! Go to Solution.
2024-12-06 12:05 PM
Could you please try to import it using the following Methode:
Go to File > Open Projects from File System... > and select the directory of your project. After that, on the Folder file select the STM32CubeIDE folder. "
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-04 11:46 AM
Hello @ZAIDS-S23
I've answered your question on this FAQ. If it solve your issue, a kudo From you on the wiki will really help to make it visible for others who have the same behavior.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-06 9:51 AM
Hi
I've taken your advice and cloned the git repo as per the answer you gave. I opened the .proj file for the Beacon, and tried building the project. I get the following error:
non constant or forward reference address expression for section .ARM.extab
Any way to solve this error?
Regards
2024-12-06 9:58 AM
Could you please open .cproject file or call it directly using the import project of the STM32CubeIDE.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-06 11:27 AM
I tried clicking on the .cproject itself and it did not open in CubeIDE.
Which option should I select to open it from the Import option?
2024-12-06 12:05 PM
Could you please try to import it using the following Methode:
Go to File > Open Projects from File System... > and select the directory of your project. After that, on the Folder file select the STM32CubeIDE folder. "
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-06 11:08 PM - edited 2024-12-07 12:40 AM
I've tried this and tried building the application, I still get the same error i.e. non constant or forward reference address expression for section .ARM.extab.
Just for reference, I am using STM32CubeIDE 1.12.1.
I've tried updating the IDE itself, which then presents the error
An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,org.antlr.runtime,4.10.1.v20230210-1433
Edit: I uninstalled STM32CubeIDE and I am trying to reinstall it. I'm not able to download an installation file for 1.17.0 from the ST website. This was also the case when trying to download STM32CubeWB.