cancel
Showing results for 
Search instead for 
Did you mean: 

Missing projects for STM23WB5MM

PStee
Associate II

I purchased the STM32WB5MM-DK and it has an application running. When I update CUBE-MX with the patch for STM23WB5MM , there are is no examples that match the application. The training talks about the example projects but they did not come with the update. Where can I find the source project for the Dev Boards application?  I work in MKS toolset 

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @PStee 

What is the training you are mentioning on your post? For the STM32WB5MM-DK, examples are available here on the STM32CubeWB V1.23.0 available on the ST website and can be uploaded directly using the STM32CubeMX. About the original example that came with the board, i remember that it was the BLE_HeartRate or the BLE_Sensor. 

Best Regards.

II

 

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @PStee 

What is the training you are mentioning on your post? For the STM32WB5MM-DK, examples are available here on the STM32CubeWB V1.23.0 available on the ST website and can be uploaded directly using the STM32CubeMX. About the original example that came with the board, i remember that it was the BLE_HeartRate or the BLE_Sensor. 

Best Regards.

II

 

STM32WB Online Training - STMicroelectronics is the training I am referring to. It is not included in the files installed with the Cube MX WB tool set. I am starting a new hardware design so the logical place to begin is the Cube MX. What other discrepancies are there between the Cube MX and the git code lines? 

Regards 

Peter