2025-10-22 5:27 AM
Hello,
I use a STM32WLE5JCI6 MCU. Sometimes I need a good clock precision so I switch to HSE as SYSCLK, with a 32MHz quartz. I use 4MHz as HCLK, and I chose to set HSEPRE=2 and HPRE=4. When I call SystemCoreClockUpdate() function the SystemCoreClock value is 8MHz, because HSEPRE value is not considered. Is it a bug or this is the expected value, for any reason I missed? The function HAL_RCC_GetSysClockFreq() uses LL_RCC_HSE_IsEnabledDiv2 to return the expected value, so the SystemCoreClock value is 4MHz if I configure the HSE as sysclock at startup.
Thanks,
Sylvain
My code:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSEDiv = RCC_HSE_DIV2;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK3|RCC_CLOCKTYPE_HCLK
|RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1
|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV8;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.AHBCLK3Divider = RCC_SYSCLK_DIV8;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
/** Enable the HSE Prescaler
*/
__HAL_RCC_HSE_DIV2_ENABLE();
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_SYSCLK, RCC_MCODIV_1);
}and:
int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
printf("Test HSE. %s - %s\n\r", __DATE__, __TIME__);
printf("SystemCoreClock = %lu\r\n", SystemCoreClock);
SystemCoreClockUpdate();
printf("SystemCoreClock = %lu\r\n", SystemCoreClock);
Result:
Test HSE. Oct 22 2025 - 13:59:06
SystemCoreClock = 2000000
SystemCoreClock = 4000000
2025-10-22 6:29 AM
Sure looks like a bug. Most chip don't have an HSEPRE field so it probably got missed.
2025-10-22 7:06 AM
Thanks for your answer. Is it safe to do this as a workaround?
/* Update the SystemCoreClock global variable */
SystemCoreClock = HAL_RCC_GetHCLKFreq();