cancel
Showing results for 
Search instead for 
Did you mean: 

_Min_Heap_Size and _Min_Stack_Size

EŞimş.1
Associate II

Hi ,

Default values of the _Min_Heap_Size and _Min_Stack_Size is setting according to What? I changed these variables from 0x200 , 0x400 to 0x00 and 0x00 resprectively ,end then no problem,no error .I guess that Static and dynamic variables in RAM are in the RAM Base Addr + (_Min_Heap_Size or _Min_Stack_Size ) . Why are they 512 byte and 1K byte as default?

0693W00000Bb7WbQAJ.png 

Best regards,

Enes.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
I gave the explanation in my first reply, so did Andrew. You just ignored it and asked the question again. Figured you wanted a more direct answer. Best of luck, I'm done here.
If you feel a post has answered your question, please click "Accept as Solution".