2023-04-03 07:34 PM
Hi Sir. Madam,
For MB1791 Development Broad, there are 3 Type of design:
But I doubt the BOM given, the part Description, Value and Manufacture Part Number are not tally for the Location: C8, C9, C26, C31:.
Pls advise the correct value for MB1791-HighBand_HighPower.
Thanks.
Solved! Go to Solution.
2024-06-06 04:57 AM
Hello @KKan.1,
Thank you for your input, the updated corrected BOM is on-line:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-07 02:20 AM
Hello @KKan.1 and welcome to ST Community
Thank you for bringing this to our attention!
I reported the issue internally.
Internal ticket number: 149284 (This is an internal tracking number and is not accessible or usable by customers)
Sarra
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-17 03:50 AM - edited 2023-11-20 08:59 AM
Hello again @KKan.1,
As mentioned earlier, documents will be updated soon with the right values, but I can inform you that the recommended value of C8, C9, C26, C31 is 6.8pF as it is mentioned in the board schematics:
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-17 05:21 PM - edited 2023-11-20 08:59 AM
Hi Sara,
Thanks for feedback.
For my understanding, Schematic is general for the 3 different Band & Power reference.
BOMs is the actual that we need to follow :
Pls advise.
2023-04-19 03:59 AM
Hello again @KKan.1
>> BOMs is the actual that we need to follow
Indeed, the BOM will be updated with the correct value 6.8pF, so you can safely use it before the update!
Hope that's clear!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-06 04:57 AM
Hello @KKan.1,
Thank you for your input, the updated corrected BOM is on-line:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.