2025-10-08 11:20 PM - last edited on 2025-10-09 12:01 AM by Andrew Neil
How I get the software stack/firmware library stack with LoRaWAN for STM32WLE5xx MCU (other than Seed Studio Library) ?. In github, stm32wl repository only has a STM32WL55JC drivers alone. Is there any possibilities to get a firmware stack for STM32WLE5xx ? If anyone have an idea kindly let me know.
2025-10-09 1:22 AM
Hello @mathiyazhagan-meteoros and welcome to the Community,
STM32CubeWL supports all STM32WL MCUs. However, examples and BSP files are available only for the NUCLEO-WL55JC board and the B-WL5M-SUBG1, which are the official STM32WL evaluation boards.
There is no evaluation board based on the STM32WLE. If you have an evaluation board based on the STM32WLE, I recommend you contacting the board or module manufacturer for additional support.