2024-04-16 03:43 PM
I'm using a custom board with the STM32WL5MOC. I've noticed that the last three 32-bit words of the OTP have been written to the values:
FF FF FF FF FE FF FF FF 02 00 10 38 D1 DB AF 46
This makes the OTP 16 bytes shorter. Is this intentional, or is it a bug?
Solved! Go to Solution.
2024-04-22 11:51 AM
Or not their job... Open a support case, or talk to your local sales rep, or FAE
https://www.st.com/content/st_com/en/support/support-home.html
2024-04-18 06:04 PM
I wonder if this is done intentionally. There doesn't seem to be any way to distinguish between the module and STM32WLE5/STM32WL5x IC. This would be helpful for me as I'm migrating from the Seeed Studio Wio-E5 that uses the WLE module. They are different in that the LSE drive strengths differ; the Seeed Studio module uses a low drive, and the STM32WL5MOC uses a high drive for the LSE. It would be nice to be able to unambiguously tell what part is needed so I can set this appropriately.
Barring that, I'll probably set the drive strength to high in both cases, and lower the drive strength once I peek inside the OTP to find the part number (that I write in manufacturing).
2024-04-22 11:48 AM
I can only assume that the module development team at ST does not read this forum...
2024-04-22 11:51 AM
Or not their job... Open a support case, or talk to your local sales rep, or FAE
https://www.st.com/content/st_com/en/support/support-home.html
2024-04-23 10:02 AM
I apologize to everyone for the snarky post. It was uncalled for. I had a fundamental misunderstanding of the purpose of the forum. In the future, I'll take the approach that @Tesla DeLorean suggested.