cancel
Showing results for 
Search instead for 
Did you mean: 

Memory issue while using "STM32WB1MMC"

KWOOJ
Associate III

During compilation with IAR, I ran into an error. Please refer to the picture below.

KWOOJ_0-1710921360010.png

 

Upon checking the source size via the map file, it appears as follows:

KWOOJ_1-1710921515091.png

 

After examining the RAM size, it seems that the capacity of SRAM1 is less than 12K. I believe this shouldn't cause a compilation error.

KWOOJ_2-1710921563171.png

 

What could be the cause of the compilation error?

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @KWOOJ 

I've carefully answered this question on this post. Please Check it if you are facing the same behavior.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @KWOOJ 

I've carefully answered this question on this post. Please Check it if you are facing the same behavior.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.