Rephrased Question:
I am working on a graduation project that involves reading values from temperature, pressure, and light sensors through a BLE service with three characteristics. I also have another service to control a fan speed through another service with a characteristic.
- I used the P2P_Server example and added a service and modified the first one, but I cannot see this service and access it, as shown in the attached image.
- The device only appears in the nRF Connect for Desktop Bluetooth Low Energy.exe program and does not show up in the ST BLE Toolbox application. What could be the problem?
- Can I name the service and characteristics with clear names instead of UUIDs? I don't mean within MX; I want the values to appear in the monitoring application, like in the HeartRateThreadX example.
Additional Details:
- I added a new service and modified the first service in the P2P_Server example.
- Despite this, I cannot see or access the service in the monitoring applications.
- The device appears in the nRF Connect for Desktop Bluetooth Low Energy.exe program but does not show up in the ST BLE Toolbox application.
Further Inquiries:
- How to name the service and characteristics with clear names that appear in monitoring applications instead of UUIDs.
- How to ensure the device appears in various BLE applications.
![AmerRiha_0-1722445117377.png AmerRiha_0-1722445117377.png](https://community.st.com/t5/image/serverpage/image-id/83686i0E3F4BA50F03A40A/image-size/medium/is-moderation-mode/true?v=v2&px=400)
![AmerRiha_1-1722445133617.png AmerRiha_1-1722445133617.png](https://community.st.com/t5/image/serverpage/image-id/83687i4630F35698100257/image-size/medium/is-moderation-mode/true?v=v2&px=400)
Please respond as soon as possible. Thank you very much.