2025-03-11 1:32 AM - last edited on 2025-03-11 1:40 AM by STTwo-32
Hello
thanks for replying.
to upload the Hex file i used STM32Programmer, but when i connect the borad via USB cable to my PC i receive un error :
Best Regards.
2025-03-11 1:50 AM
Hello @ljm
Could you please try to follow this procedure:
PS: Make sure to use the STM32CubeProgrammer V2.19.0
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-12 12:16 AM
Hello,
Thank you for replying
i have an issue to connect the board to STM32Cube programmer
thanks
2025-03-12 12:51 AM
Have you followed the steps I've mentioned in my previous post.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-12 1:18 AM
hello
thanks for replying, i change my USB cable and it works, but when i used STM32CubeMonitorRF , can't connect
thanks
2025-03-12 1:22 AM
Have you followed the steps on this post:
Connecting the NUCLEO-WB05KZ to STM32CubeMonitorRF - STMicroelectronics Community
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-12 1:52 AM
Hello
thanks for relying
it works thank you very much.
one last question please here why "Get RSSI" is locked ? i want to get the RSSI value
thanks