cancel
Showing results for 
Search instead for 
Did you mean: 

Issue connecting the NUCLEO-WB05KZ to the STM32CubeProgrammer

ljm
Associate III

Hello

thanks for replying.

to upload the Hex file i used STM32Programmer, but when i connect the borad via USB cable to my PC i receive un error : 

ljm_0-1741681923679.png

Best Regards.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @ljm 

Could you please try to follow this procedure:

  • If it is the first time you will program the board, follow the recommendation of the note on the chapter 7.12 of the STM32WB05 Nucleo-64 board (MB1801 and MB2032) - User manual and don't forget to click on the reset button before connecting to the STM32CubeProgrammer if the LD2 is still toggling.
  •  If you are used to program the board, try to fit the jumper on both pins 7 and 5 on the CN3 of the board and connect the board using the Hot plug mood

PS: Make sure to use the STM32CubeProgrammer V2.19.0

 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
STTwo-32
ST Employee

Hello @ljm 

Could you please try to follow this procedure:

  • If it is the first time you will program the board, follow the recommendation of the note on the chapter 7.12 of the STM32WB05 Nucleo-64 board (MB1801 and MB2032) - User manual and don't forget to click on the reset button before connecting to the STM32CubeProgrammer if the LD2 is still toggling.
  •  If you are used to program the board, try to fit the jumper on both pins 7 and 5 on the CN3 of the board and connect the board using the Hot plug mood

PS: Make sure to use the STM32CubeProgrammer V2.19.0

 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

Thank you for replying

i have an issue to connect the board to STM32Cube programmer 

ljm_0-1741763783933.png

thanks

Have you followed the steps I've mentioned in my previous post.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

hello

thanks for replying, i change my USB cable and it works, but when i used STM32CubeMonitorRF , can't connect 

ljm_0-1741767419979.png

thanks

Have you followed the steps on this post:

Connecting the NUCLEO-WB05KZ to STM32CubeMonitorRF - STMicroelectronics Community

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello

thanks for relying

it works thank you very much.

one last question please here why "Get RSSI" is locked ? i want to get the RSSI value 

ljm_0-1741769523869.png

 

thanks