2023-08-28 3:15 AM
Hi Team,
Any Transceiver IC support up to 3GHz range in STMicroelectronics? And how to interface with controller.!
Thanks and Reguad,
Aravind
Solved! Go to Solution.
2023-08-28 5:59 AM
shure, read the ds.
but for beginner...better look at ready evaluation board, -> ADRV9364-Z7020
2023-08-28 5:18 AM - edited 2023-08-28 5:19 AM
Hello @Aravind
I suggest you to take a look on the STM32WB that works on the frequency of 2.4GHz. But, working on the 3GHz need to have your own concept of technology because classic technologies cover the sub-ghz bands such as LoRa, the 2.4ghz such as Bluetooth and Wi-Fi and the band between 3.1GHz and 9GHz for the UWB technology.
Hope this is helpful for you. If your question is answered please check this answers as a best answer to be diffused.
Best regards.
II
2023-08-28 5:42 AM
Hi Issamos,
Thanks for your reply,
Now I want to configure the AD9364 with any other controller ,if it is possible?
Thanks and regards
2023-08-28 5:59 AM
shure, read the ds.
but for beginner...better look at ready evaluation board, -> ADRV9364-Z7020
2023-08-28 6:10 AM
In this evaluation board is using FPGA .I want to implemented in microcontroller only.And AD9364 RF Transciver implemented any controller.
It is possible to implement?
Thanks and regards
2023-08-28 6:25 AM
2023-08-28 7:00 AM - edited 2023-08-28 7:02 AM
2023-08-28 7:08 AM
you choose a super fast transceiver, so need high data in/out speed, usually best possibly with fpga .
depends on...what you wanna do with it ? frequ.span ? speed ? data rate ? continuous/real time ?