2021-02-06 2:22 AM
I wanted to use an additional Pin in the Ping Pong LoRa example program for the nucleo-WL55JC1 Board. So i set one as Output and saved the Configuration file. What happened, was that my Project then had about 200 Errors. Saving the Configuration must have changed something realy essential. So how do i add Pins properly without changing the rest of the already made Project?