‎2021-03-10 09:56 AM
How may I obtain the P-Nucleo-LRWAN2 pack, my special interrest is the Gateway.
Solved! Go to Solution.
‎2021-03-17 08:00 AM
registration not confirmed...
‎2021-03-16 01:41 AM
Please, see link for google drive repository of STM32WL workshop, see Slides folder for 5_STM32WL_WS_hands-on_Lorawan.pdf
https://drive.google.com/drive/folders/19MvsUnujddCwi5wH939zRJH6jf-XvD5Z
‎2021-03-16 03:08 AM
LoRaWAN_End_Node is an empty folder ?
‎2021-03-16 06:57 AM
Yes, indeed, it is empty as target folder for the project creation during relevant hands-on. All the needed steps are described in slide set, I've pointed.
‎2021-03-16 07:20 AM
Many thanks to share this hands-on.
Are there also hands-on available for the I-NUCLEO-LRWAN1 ?
I struggle with te AT-commands on (WM-SG-SM-42_Shield_V1.0)
Best regards, Erik
‎2021-03-16 07:27 AM
Please, download the I-CUBE-LRWAN repository
and see "AT_Master" example for STM32L073RZ-Nucleo
Please, consider the module populated on the top of WM-SG-SM-42_Shield_V1.0 is AT-cmd driven Lorawan modem manufactured by USI (it is NOT ST module but ST MCU is inside), link to resources is below
‎2021-03-16 07:28 AM
Board WM-SG-SM-42_Shield_V1.0 is out of the scope of STM32WL workshop, just to clarify.
‎2021-03-16 07:31 AM
OK, thanks
‎2021-03-16 08:01 AM
Would it be possible to send me the STM32 LoRa-enabled SoC hands-on kit?
My adress is Auwegemvaart 64
2800 Mechelen
or ...
Skeyes, Erik Cool
Tervuursesteenweg 303
B-1820 Steenokkerzeel
‎2021-03-16 08:05 AM
=)