cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to acces the repository for the LRWAN2 hands-on, eventually would you send me the slides also? Many thanks in advance, Best Regatds, Erik

ECool.1
Associate III

How may I obtain the P-Nucleo-LRWAN2 pack, my special interrest is the Gateway.

1 ACCEPTED SOLUTION

Accepted Solutions
ECool.1
Associate III

registration not confirmed...

View solution in original post

14 REPLIES 14
Bartosz BORYNA
ST Employee

Please, see link for google drive repository of STM32WL workshop, see Slides folder for 5_STM32WL_WS_hands-on_Lorawan.pdf

https://drive.google.com/drive/folders/19MvsUnujddCwi5wH939zRJH6jf-XvD5Z

LoRaWAN_End_Node is an empty folder ?

Bartosz BORYNA
ST Employee

Yes, indeed, it is empty as target folder for the project creation during relevant hands-on. All the needed steps are described in slide set, I've pointed.

Many thanks to share this hands-on.

Are there also hands-on available for the I-NUCLEO-LRWAN1 ?

I struggle with te AT-commands on (WM-SG-SM-42_Shield_V1.0)

Best regards, Erik

Bartosz BORYNA
ST Employee

Please, download the I-CUBE-LRWAN repository

https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/i-cube-lrwan.html

and see "AT_Master" example for STM32L073RZ-Nucleo

Please, consider the module populated on the top of WM-SG-SM-42_Shield_V1.0 is AT-cmd driven Lorawan modem manufactured by USI (it is NOT ST module but ST MCU is inside), link to resources is below

https://github.com/USILoRaModule/USI_I-NUCLEO-LRWAN1 

Bartosz BORYNA
ST Employee

Board WM-SG-SM-42_Shield_V1.0 is out of the scope of STM32WL workshop, just to clarify.

ECool.1
Associate III

OK, thanks

ECool.1
Associate III

Would it be possible to send me the STM32 LoRa-enabled SoC hands-on kit?

My adress is Auwegemvaart 64

2800 Mechelen

or ...

Skeyes, Erik Cool

Tervuursesteenweg 303

B-1820 Steenokkerzeel

ECool.1
Associate III

=)