cancel
Showing results for 
Search instead for 
Did you mean: 

I-CUBE-LRWAN v2.0.0 with Nucleo-L073RZ board and I-Nucleo-LRWAN1 shield

Nucleo-L073RZ board and I-Nucleo-LRWAN1 (USI module) shield - as supplied as the "Sensor" part of the P-NUCLEO-LRWAN2 kit:

0693W00000Bca5WQAR.png 

The documentation refers to I-CUBE-LRWAN at v1.2.2; in v2.0.0 (March 2021), the directory structure has changed somewhat.

I assume the correct path for the "Sensor" node project is now:

Projects\NUCLEO-L073RZ\Applications\LoRaWAN\LoRaWAN_AT_Master\STM32CubeIDE\I_NUCLEO_LRWAN1

Can anyone confirm if this actually works?

At the moment, mine doesn't seem to be sending any AT commands from the Nucleo board to the USI shield...

43 REPLIES 43

So that is a different question, and relates to a different version - you should start a new thread for that.

ELeit.3
Associate II

Hi, I'm Erton and purchase a P-nucleo-LRWAN2 and i can't run any exemples on STM32CubeExpansion_LRWAN_V2.1.0, my board and shield is a L073RZ and I-NUCLEO-LRWAN1.

In my case, i disable debug and now is my teraterm is

0693W00000NpzErQAJ.pngI noticed the index #USE_I_NUCLEO_LRWAN1 is gray in all code. I try rebuild the index but

unsuccessfully. Can someone help me?

Best Regards!!!

EDIT

My firmware version of I-NUCLEO_LRWAN1 is 4.0.2.

@ELeit.3​  - "STM32CubeExpansion_LRWAN_V2.1.0"

The original thread is nearly a year old, and was about v2.0.0 - so I think it would be better to start a new thread.

You can always give a link to this thread, for reference...

(also a link here to your new thread - so people will find it)