cancel
Showing results for 
Search instead for 
Did you mean: 

I can't find radio library files for coding B-L072Z-LRWAN1 module after create a project with CubeMX.

Selim Sagir
Associate III

Hello,

I choose in board selector to B-L072Z-LRWAN1 kit and create a project. But i cannot reach radio modules in TrueStudio, but only hal files. Should i add files myself, if so which files.

Thanks.

1 REPLY 1
d.hinojosa.cordova
Associate II

My advice is to use the test codes (STM32CubeExpansion_LRWAN_V1.2.1), open the projects in either IAR, KEIL or SW4STM32 and edit them for your needs.

Cheers.