2022-10-01 08:11 AM
Please disregard the first question as the answer seems to be that the WL has dual cores so it has both an M4 and an M0+.
Solved! Go to Solution.
2022-10-01 08:51 AM
WL and WB is SOCs and one core M0 is for internal hw control. Your user is M4
2022-10-01 08:51 AM
WL and WB is SOCs and one core M0 is for internal hw control. Your user is M4
2022-10-01 09:11 AM
Makes sense, @MM..1. Thanks for the timely response.
2022-10-02 11:49 PM
WB and WL product lines are both dual core with CM4 and CM0+. There is a slight difference between them: