cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up BLE AT Client on B-U585I-IOT02A?

juyec
Associate II

Hello!

I'm attempting to set up the BLE AT Client example in the STM32U5 firmware package on a B-U585I-IOT02A board. I've managed to flash it, but when I run it on the debugger (through the ST-Link v3 USB port), the "AT" and "AT+BLE_SVC=1" commands sent to the STM32WB module both return error messages.

I'm thinking it's something to do with how I originally configured the hardware, but I've been stuck for a while on it. Does anyone happen to have any ideas or fixes?

Thank you,

Jake U.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Remy ISSALYS
ST Employee

Hello,

I answered you on your previous post, BLE_MultiAppAt application isn't compatible with BLE_AT_Client example. So, if you didn't flash BLE_AT_Server application on the STM32WB5MM module, BLE_AT_Client example didn't work.

Best Regards

AUguc
Associate

Why is it inserted in board's examples!?