cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up an eddystone beacon on a B-L072Z-LRWAN1

MBour.2
Associate II

Hello,

I'm working on a project in which I want to connect to a tag that sends a Bluetooth signal with a L072Z-LRWAN1 board having a STM32L072CZYx MCU and the SPBTLE-RF Bluetooth component. There is the X-CUBE-BLE1 software pack that could help me realize that but I don't quite understand which application should I use. I think the eddystone beacon is the most appropriate but there is no tutorial or explanation on how to use the functions related to that. All I want is to connect to my tag and I cannot find this particular function and I really don't understand the settings of the beacon. For example when they ask you to configure a MAC address, is it the MAC address of my module or of my tag?

If anyone knows anything regarding the BLE topic please let me know.

Thanks,

Mohamed

0 REPLIES 0