cancel
Showing results for 
Search instead for 
Did you mean: 

How to set the firmware using X-CUBE-MATTER's SBSFU on the Sleepy end device

AkihiroN
Associate III

We are developing a Matter device using X-CUBE-MATTER.

How can I make the sample firmware using SBSFU into a sleepy end device? Just setting CFG_FULL_LOW_POWER to 1 fails the commissioning. How can I enable Sleep Mode like the generic-switch app?
The development environment is as follows.
Hardware: STM32WB5MMG-DK
Firmware: Window-App-SBSFU
X-CUBE-MATTER Version: 1.1
Implementation CFG_FULL_LOW_POWER is set to 1

0 REPLIES 0