How to send packet between mesh nodes by BLE_MeshLightingDemo Example.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-28 10:59 PM
Hi Sir:
I try to use BLEMesh_SetRemoteData(..) with Unicast Address from BLEMesh_GetAddress() for sending packets between two nodes, but the received node dosn't call the Vendor_WriteLocalDataCb().
Is there any suggestion for me to send the packets with manually fiiled payload between Mesh nodes ?
Thanks,
Jack
- Labels:
-
BLE Mesh
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-29 2:17 AM
Hi Jack,
What is the use case ? What do you mean by sending packets ?
Just for information, Bluetooth Mesh packet sizes are 15 bytes for unsegmented messages (unack'd/unreliable), however, it is also possible to send a segmented/reliable message which can consist of 12 bytes per packet (3 byte packet overhead for segmentation) with a 32 segment max, which would yield a 384 byte total message size.
Obviously, segmented messages are much slower than unsegmented due to the required ack'd response from the receiver.
It is not possible to send 1KBs in a single packet or even feasible to send over multiple messages.
You should note that Bluetooth mesh in its current version (v1.0) is primarily targeted at command/control type applications and therefore the concept of flooding 1K bytes across the mesh is not a primary or expectant use case.
Hopefully Mesh v1.1 will deliver an additional bearer layer which incorporates advertising extensions and additional throughput enhancements, to be confirmed.
Best regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-29 7:51 AM
Jack,
Before the 2 nodes has to be provisioned, and configured with the smartphone Mesh application.
The Client node have to be configured as a publisher to the Server node.
The Server node have to be configured as a subscriber to the Client node.
On the application SW side before using the BLEMesh_SetRemoteData() function, you have to get the publish address (a provisioned node can publish to One node or Group) with the BLEMesh_GetPublishAddress() function.
BLEMesh_GetAddress() function give the address of the node that will publish, no the publication address node.
You have an example of the functions use in the function BLEMesh_ModelsCommand() of the models_if.c file.
This function is called each time there is a short SW1 button press.
Best regards.
Best regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-29 8:57 PM
Hi Eric:
Thank you for your information, but I am not familiar with BLE mesh.
So I still have few questions!
(1)
I have two nodes provisioned, and the send message like below.
Can I send the message like this?
Send Node:
Unicast Address: 0x0003 from BLEMesh_GetAddress()
TX:
#define TX_DATA_LEN 5
MOBLEUINT8 tx_data[TX_DATA_LEN] = {0x00, 0x01, 0x02, 0x03, 0x04};
MOBLEUINT32 tx_data_len = TX_DATA_LEN;
BLEMesh_SetRemoteData(0x0004, 0x00, APPLI_LED_CONTROL_STATUS_CMD, tx_data, tx_data_len, MOBLE_TRUE, MOBLE_FALSE);
Receive Ndoe:
Unicast Address: 0x0004 from BLEMesh_GetAddress()
RX:
MOBLE_RESULT Vendor_WriteLocalDataCb(MOBLE_ADDRESS peer_addr,
MOBLE_ADDRESS dst_peer,
MOBLEUINT8 command,
MOBLEUINT8 const *data,
MOBLEUINT32 length,
MOBLEBOOL response)
{
// Not going into here...
}
(2) How to configure Client/Sever Node to publisher/subscriber ?
Best regards,
Jack
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-01-26 11:10 PM
Hi EMECH,
How to send and receive segmented message?
Correct me if I am wrong. If I send 100 bytes of segmented message, means that BLE Mesh handle all internal communication and on receiver I get complete data of 100 bytes?
And one more question, is it possible to write "default provision data" by user application from CortexM4 STM32WB? I want to avoid use smartphone to configure each node.
Best Regards