2024-06-25 10:18 PM
Hi,
I want to use BLE mesh to reach my application, the requirements below.
Based on the above needs, are there any related projects that can be referred to?
Please help me and give the suggestions.
Thanks.
Solved! Go to Solution.
2024-06-26 02:06 AM
Hello @Cooper_WJH and welcome to the ST Community
I suggest you refer to:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-26 02:06 AM
Hello @Cooper_WJH and welcome to the ST Community
I suggest you refer to:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-26 02:29 AM
2024-06-26 05:15 AM
I suggest you first to look at one of those 3 examples from the same Firmware:
and do the necessary modification to adapt it to your needs. If you are looking for a support dedicated to this special use case, you can contact one of our local FAEs that can guarantee a dedicated support for the details of your use case.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-04 10:34 PM
I have started using the "BLE_MeshLightingPRFNode" example test with the "ST BLE MESH" APP.
And I want to try to use the "data in" & "data out" characteristics in GATT "provisioning service" & "proxy service" to control the mesh network and trace the interaction in the code.
However, I cannot find any documentation or examples about how to use these services, like the data or packet format for writing the data to the specific node to control, etc.
Is there any example or guideline about these?
2024-07-04 11:25 PM
Hello @Cooper_WJH
This is a new question. I suggest you select a best answer for this post and open a new one and add more details about your use case and what exactly you need so the community members may help you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.