How to enter stop2 mode in stm32wb, when the Ble stack opened?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-18 3:41 AM
According to the subject, I found I can't enter to the stop2 mode ,when i run the ble stack (APPE_Init() ) in p2p_server. I tried to use HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI); behind the aci_gap_set_non_discoverable(); but it wasn't worked . What program i need to add?
Thank you very much.
​
Solved! Go to Solution.
- Labels:
-
Power
-
STM32WB series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-26 3:54 AM
Hello,
You should no add any code to enter stop mode 2. I am not sure where you added SCH_Run(0) but wherever this was added, please remove it.
I would suggest to start from the p2p_sever example as it has been delivered without any code change and modify the setting in app_conf.h to have
Set CFG_DEBUGGER_SUPPORTED to 0
Set CFG_DEBUG_BLE_TRACE to 0
Set CFG_DEBUG_APP_TRACE to 0
To make sure the device enter low power mode, you may output the system clock on the MCO ouput and check the signal with either an oscilloscope or a digital analyzer. When the device enters Stop Mode, you should see the clock not toggling anymore in between advertising packets.
You may use HAL_RCC_MCOConfig(uint32_t RCC_MCOx, uint32_t RCC_MCOSource, uint32_t RCC_MCODiv) to ouput the system clock on MCO.
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-20 4:22 AM
Hello,
The only thing to do to make a BLE application running with the best power consumption is to change the default settings in app_conf.h
All BLE applications are keeping the debugger and traces enable to help the user to implement and debug his application
The BLE_HearRate is the only one which is by default configured to provide by default the best power consumption.
You may check the differences between the two app_conf.h files but basically, you need to
Set CFG_DEBUGGER_SUPPORTED to 0
Set CFG_DEBUG_BLE_TRACE to 0
Set CFG_DEBUG_APP_TRACE to 0
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-23 7:40 PM
Thank you very much. I Tried to check the BLE_HeartRate example and changed the app_conf.
The program entered the low power mode when Ble tasks ran in SCH_Idle, but i found that
the mcu in stop mode after running ble stack which power consumption is ten times larger than
mcu in stop mode before running ble stack . Is it possible to turn off only the part of BLE?
​
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-24 4:09 AM
Hello,
The p2p_server application is advertising at startup. It depends which tool you are using to make power measurement.
Between advertising packets, the STM32WB should enter Stop Mode 2. In that case the power consumption is in the range of 2.8uA.
When the device advertises, the Radio is transmitting and the power consumption increases to several mA.
The tool you are using to make power measurement may not be able to make correct power measurement with a power switch from some few uA to few mA.
This is most of the time the case with multimeter and the average power measurement reported is not correct.
Could you please confirm which tool you are using to make power measurement ?
This shield below is providing very accurate power measurements
https://www.st.com/en/evaluation-tools/x-nucleo-lpm01a.html
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-26 3:14 AM
Thank you.
I want to enter the stop2 mode after device stopping advertising (aci_gap_set_non_discoverable(); ),
so I have followed the example code and added SCH_Run(0) after device stopping advertising in order to enter
he SCH_Idle() and stop2 mode.
​
I use multi-meter to measure the current which was 4.3 mA on JP2 of Nucleo-68 board.
It is a lot different from the spec.
​
I think that the MCU didn't enter the low power mode.
​
Which part do i need to modify?
Regards.
​
​
​
​
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-26 3:54 AM
Hello,
You should no add any code to enter stop mode 2. I am not sure where you added SCH_Run(0) but wherever this was added, please remove it.
I would suggest to start from the p2p_sever example as it has been delivered without any code change and modify the setting in app_conf.h to have
Set CFG_DEBUGGER_SUPPORTED to 0
Set CFG_DEBUG_BLE_TRACE to 0
Set CFG_DEBUG_APP_TRACE to 0
To make sure the device enter low power mode, you may output the system clock on the MCO ouput and check the signal with either an oscilloscope or a digital analyzer. When the device enters Stop Mode, you should see the clock not toggling anymore in between advertising packets.
You may use HAL_RCC_MCOConfig(uint32_t RCC_MCOx, uint32_t RCC_MCOSource, uint32_t RCC_MCODiv) to ouput the system clock on MCO.
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 1:35 AM
Thanks .
Can program jump out to the Ble scheduler ?
​
I want to close Ble stack and do another application.
​
Then , the mcu will reset the Ble stack and run Ble application.
​
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 3:46 AM
I find that ​I must add LL_AHB2_GRP1_ReleaseReset(); to clear the ouput interrupt ping
before go to stop mode .
Then, the system will go into low power.
Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 4:10 AM
Hello,
From now I will rename scheduler into sequencer because that's the way it is documented in the AN and how this will be delivered in the coming v1.2.0 release.
The sequencer implements a basic baremetal while() loop where each function that you would like to be called in the background while loop shall be first registered and then triggered with UTIL_SEQ_SetTask().
Based on this, you cannot jump out from the sequencer as this would mean jumping out from the background while loop.
However, as long as the stack is not triggered , it will not be executed so this is matching the behavior you would like to see eg no ble activity and no ble application running in background.
There is no need to close the Ble Stack. As long as there is no BLE activity, the CPU2 Ble subsystem will be in low power and will not burn any power than as if it has never been started.
So, when you do not need anymore BLE, you dont have something specific to be done with the ble stack to enter stop mode. As long as you have no more ble activity ( no scan, no advertize, no connetcion ), the BLE susbystem will burn no power.
If you need to run another application in background, just register it to the sequencer and call UTIL_SEQ_SetTask() each time you need it to be executed once in the background.
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 4:15 AM
Hello,
I believe in that case you were entering stop mode ( eg if you monitor the system clock on the MCO, you should see some time that it does not run).
The power consumption was very likely due to a wrong GPIO setting that was driving current.
Calling LL_AHB2_GRP1_ReleaseReset() before entering Stop Mode may not suit your application because this will demux all your peripheral (UART, SPI, etc..) that you may have configured upfront.
I would suggest to identify which IO was driving current and fix it.
Regards.