2022-11-22 11:59 PM
The project is running on FreeRTOS in the CMSIS_V2 mode.
I need to have a BLE custom template to configure my own services and characterisctics.
In the case with the FreeRTOS running, I can just enable the BLE SIG Heartrate. The other BLE Applications are not present. But, if I disable the RTOS, then all the BLE applications are available.
Is there any way to enable both RTOS and the BLE Custom template?
Thanks in advance.
MCU used: STM32WB55
Dev board: P-Nucleo WB55
2025-02-11 1:13 AM
Hello,
Have you managed to do something with this ?