2024-08-03 12:16 AM
I have configured a BLE MESH with two nodes one as client and other as server . It is working well .
I also want to recieve the same data that is being exchanged on Phone. Can someone tell me how this can be done and what app I must use.
Solved! Go to Solution.
2024-08-10 12:07 PM
To do this just flash any MESH MODEL SENSOR application to th dev boards . in the configuration header file comment the client define and remove the slash from server model.
Turn on both the devices . Go for provsioning ,I have done this with STM32WB5MM-DK .Here is the process. Open a terminal like tera term or Hterm and then setup the port baud rate 9600 . After this click on reset and B1 together and release reset . Once you relese reset hold B1 and you will see the Blue LED blinks once it blink Check the BLE MESH APP now . On the right edge click on + and just get done with setting up both devices . Once added go into model section and then click on B1 on server and you will get tempreture on phone as well as client hold B1 for distance . Other important parts are simply in the read me file.
2024-08-07 2:52 AM
solved
2024-08-08 8:45 AM
Hello @Rituraj
Please add your solutions. It may help someone else having same problem.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-10 12:07 PM
To do this just flash any MESH MODEL SENSOR application to th dev boards . in the configuration header file comment the client define and remove the slash from server model.
Turn on both the devices . Go for provsioning ,I have done this with STM32WB5MM-DK .Here is the process. Open a terminal like tera term or Hterm and then setup the port baud rate 9600 . After this click on reset and B1 together and release reset . Once you relese reset hold B1 and you will see the Blue LED blinks once it blink Check the BLE MESH APP now . On the right edge click on + and just get done with setting up both devices . Once added go into model section and then click on B1 on server and you will get tempreture on phone as well as client hold B1 for distance . Other important parts are simply in the read me file.