cancel
Showing results for 
Search instead for 
Did you mean: 

help with porting files from STM32F429ZI project to STM32WBRG55

JGhaz.1
Associate

this error showed when i build the project

```

c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: C:\Users\gjallouli\STM32CubeIDE\ETO\ETO_FW_Production_Pack\Core\Src\dwt_uwb_driver\lib\libdwt_uwb_driver-hfp-5.8.0.a(deca_compat.c.obj): in function `dwt_probe':

deca_compat.c:(.text.dwt_probe+0x94): undefined reference to `__dw_drivers_start'

c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: deca_compat.c:(.text.dwt_probe+0x98): undefined reference to `__dw_drivers_end'

```

when i searched the '__dw_drivers_start' only exists in the flash of F4 .

can i modify the flash of WB and create other sections

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Markus GIRDLAND
ST Employee

Yes, you can create sections as you please in the linker script of the WB.

Is this symbol supposed to be defined in the linker script or in the a library or in c code?

it's supposed to be defined in the linker script