cancel
Showing results for 
Search instead for 
Did you mean: 

HeartRate FreeRTOS Default task

ABN
Associate III

Hi all,

I'm referring to BLE_HeartRateFreeRTOS example project. As per my understanding, controller wakes up to advertise based on the Adv Interval. This can be fast(80ms-100ms) or low power advertising(1s-2.5s).

In this project there is a default task, which gets initialized and is run on boot up. This default task is not running after subsequent wakeup of controller. May I know, how can I make this default task to run??

Also is there any FreeRTOS, STOP2 mode and BLE Beacon based example project available?

0 REPLIES 0