2023-11-23 08:41 AM
hi all
I'm working on a P-NucleoSTM32WB board
I've try BLE_p2pServer_Ext exemple with CM0 loaded with stack_full_extended.bin and it works well
on the other hand I've a simple Custom app that works well
after tweaking .ld file for getting it to work with extended stack on CM0 it works ok
I've added adv_ext_app.c/h from exemple but at ADV_EXT_Start() call the
hci_le_read_number_of_supported_advertising_sets(&adv_set_count_supported)
returns status 1 (Unknown HCI command)
I've isolated this in a button press call and it's same
void Custom_Switch1_Action(void)
{
APP_DBG_MSG("-- Switch 1 \n");
APP_DBG_MSG(" \n\r");
tBleStatus status = BLE_STATUS_INVALID_PARAMS;
uint8_t adv_set_count_supported;
uint8_t HCI_Version;
uint16_t HCI_Subversion;
uint8_t LMP_Version;
uint16_t Company_Identifier;
uint16_t LMP_Subversion;
status = hci_read_local_version_information(&HCI_Version,&HCI_Subversion,&LMP_Version,&Company_Identifier,&LMP_Subversion);
APP_DBG_MSG("Hci Version Read status %u \n HCI_Version \t%u \n HCI_SubVersion \t%u \n LMP_Version \t%u \n Company Id \t%u\n LMP_SubVersion \t%u\n",
status ,
HCI_Version,
HCI_Subversion,
LMP_Version,
Company_Identifier,
LMP_Subversion);
status = hci_le_read_number_of_supported_advertising_sets(&adv_set_count_supported);
APP_DBG_MSG("Supported Adv Set Count Status %u \n Adv Supported : %d\n",status ,adv_set_count_supported);
}
this task is well registered in HCI calling tasks
/**< Add in that list all tasks that may send a ACI/HCI command */
typedef enum
{
CFG_TASK_ADV_CANCEL_ID,
#if (L2CAP_REQUEST_NEW_CONN_PARAM != 0 )
CFG_TASK_CONN_UPDATE_REG_ID,
#endif
CFG_TASK_HCI_ASYNCH_EVT_ID,
/* USER CODE BEGIN CFG_Task_Id_With_HCI_Cmd_t */
CFG_TASK_SW1_BUTTON_PUSHED_ID,
CFG_TASK_SW2_BUTTON_PUSHED_ID,
CFG_TASK_SW3_BUTTON_PUSHED_ID,
/* USER CODE END CFG_Task_Id_With_HCI_Cmd_t */
CFG_LAST_TASK_ID_WITH_HCICMD, /**< Shall be LAST in the list */
} CFG_Task_Id_With_HCI_Cmd_t;
void Custom_APP_Init(void)
{
/* USER CODE BEGIN CUSTOM_APP_Init */
UTIL_SEQ_RegTask(1<< CFG_TASK_SW1_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, Custom_Switch1_Action);
UTIL_SEQ_RegTask(1<< CFG_TASK_SW2_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, Custom_Switch2_Action);
UTIL_SEQ_RegTask(1<< CFG_TASK_SW3_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, Custom_Switch3_Action);
/* USER CODE END CUSTOM_APP_Init */
return;
}
and the result is
[custom_app.c][Custom_Switch1_Action][84] -- Switch 1
[custom_app.c][Custom_Switch1_Action][85]
[custom_app.c][Custom_Switch1_Action][97] Hci Version Read status 0
HCI_Version 12
HCI_SubVersion 117
LMP_Version 12
Company Id 48
LMP_SubVersion 8821
[custom_app.c][Custom_Switch1_Action][105] Supported Adv Set Count Status 1
Adv Supported : 0
if I flash back BLE_p2pServer_Ext exemple all works well
to tweek .ld file and addapt my app to Full_Extended stack I've folowed this wiki page
https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_Wireless_Stack#STM32WB5x-2FSTM32WB3x
I've missed something but what ??
thank's for any help
2023-11-29 09:04 AM
Hello,
An application has to give some specific parameters to the stack to use extended advertising. These parameters are located in app_conf.h file.
Can you check these points in your application?
You can refer to the following wiki page for more information on STM32WB Bluetooth® LE advertising extensions.
Best Regards