2020-10-15 01:48 AM
I got some STM32WB55CG samples from st office and the date code is 034. The read out FUS version is 1.1.0. Has the default firmware been upgraded? So the customer doesn't have to upgrade FUS anymore?
D:\Program Files\STMicroelectronics\stm32cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -r32 0x20030030 4 -r32 0x20030024 50
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0
-------------------------------------------------------------------
ST-LINK SN : 32FF6C063047463341421351
ST-LINK FW : V2J37S7
Board : --
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x495
Revision ID : Rev Y
Device name : STM32WBxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M0+/M4
Reading 32-bit memory content
Size : 4 Bytes
Address: : 0x20030030
0x20030030 : 01010100
Reading 32-bit memory content
Size : 52 Bytes
Address: : 0x20030024
0x20030024 : A94656B9 00000001 01010000 01010100
0x20030034 : 00000006 00000000 00000000 00000000
0x20030044 : 00000000 00000000 00658473 0080E126
0x20030054 : 00000496
Solved! Go to Solution.
2020-10-15 02:53 AM
The trend is to have all devices pre-loaded with FUS v1.1.1 in the mean term but the process is done step by step, line by line, package by package, ...
So it is hard to give you an exact answer as it depends on what type of WB devices and when you'll purchase them.
2020-10-15 01:58 AM
Considering the result of the read access at address 0x20030030, the FUS version is v1.1.1. So it is really the most up to date one.
You don’t have to do anything regarding a FUS update.
2020-10-15 02:02 AM
Im sorry, but last FUS version is 1.1.0 not 1.1.1. or am I confusing something?
2020-10-15 02:08 AM
Last official FUS version is v1.1.0 (released in the last CubeWB FW package) . But there is an internal version v1.1.1 that exists internally. As you got the chips directly from ST office, they may have been upgraded with this internal version before you get them.
2020-10-15 02:39 AM
Ok, thanks for responce, Remi.
2020-10-15 02:41 AM
So when it comes to bulk purchase in the future, what FUS default version programmed in it?
2020-10-15 02:53 AM
The trend is to have all devices pre-loaded with FUS v1.1.1 in the mean term but the process is done step by step, line by line, package by package, ...
So it is hard to give you an exact answer as it depends on what type of WB devices and when you'll purchase them.
2020-10-15 03:01 AM
Ok, thanks , Remi.
2020-10-15 03:01 AM
we have 1200 chips 512k flash and all have FUS 0.5.3 version, but we bought them for a long time ago
2020-10-15 03:05 AM
Ok this is the expected FUS version on such devices when bought some time ago.