2021-06-17 01:50 AM
Hello,
I have a question concerning STM32WB55 MCU. We are using it, and use SWD as debug, without advanced debug features (traces).
We are now facing complex bugs, and I would like to activate traces on that MCU for the M4 Core.
We do not have TRACE pins routed, so ETM use is not possible. I have seen that ETB/MTB (Embedded Trace Buffer/Micro Trace Buffer) can be activated. If I understand well, this allows core to trace little amount of instructions execution, in a RAM area, which is dumped by the debugger.
I did not managed to get it work, but it seems that this ETB/MTB is not available for that MCU. Can someone confirm ?
Is there other mean of advanced debugging, to better know execution history before a crash ? Other than classic SWO printf.
Thanks a lot
Camille
2021-07-17 09:31 AM