2019-10-16 10:00 AM
I'm using a WB55 Nucleo board and setting up a BLE connection with a 2nd WB55 Nucleo board using aci_gap_create_connection(). The connection succeeds and I am able to transfer data between the 2 boards. I would then like to terminate the connection. I call aci_gap_terminate_gap_proc(0x40) to do this, but I always get a return value of 0x46, which corresponds to BLE_STATUS_NOT_ALLOWED.
Any ideas why the call to aci_gap_terminate_gap_proc() fails? Or is there a different recommended way to terminate the BLE connection?
Thanks...
Solved! Go to Solution.
2019-10-16 01:18 PM
Hi.
"aci_gap_terminate_gap_proc" uses for terminate the specified GATT procedure, in your case, you want to terminate procedure "GAP_DIRECT_CONNECTION_ESTABLISHMENT_PROC".
Since the connection already exists, the procedure is not performed.
To terminate connection you need to call :
aci_gap_terminate(uint16_t Connection_Handle, uint8_t Reason).
In "Connection_Handle" parameter you need pass current connection handle and in "Reason" parameter pass one from list:
- 0x05: Authentication Failure
- 0x13: Remote User Terminated Connection
- 0x14: Remote Device Terminated Connection due to Low Resources
- 0x15: Remote Device Terminated Connection due to Power Off
- 0x1A: Unsupported Remote Feature
- 0x3B: Unacceptable Connection Parameters
Best regards,
Vaycheslav.
2019-10-16 01:18 PM
Hi.
"aci_gap_terminate_gap_proc" uses for terminate the specified GATT procedure, in your case, you want to terminate procedure "GAP_DIRECT_CONNECTION_ESTABLISHMENT_PROC".
Since the connection already exists, the procedure is not performed.
To terminate connection you need to call :
aci_gap_terminate(uint16_t Connection_Handle, uint8_t Reason).
In "Connection_Handle" parameter you need pass current connection handle and in "Reason" parameter pass one from list:
- 0x05: Authentication Failure
- 0x13: Remote User Terminated Connection
- 0x14: Remote Device Terminated Connection due to Low Resources
- 0x15: Remote Device Terminated Connection due to Power Off
- 0x1A: Unsupported Remote Feature
- 0x3B: Unacceptable Connection Parameters
Best regards,
Vaycheslav.
2019-10-16 01:33 PM
Hi Vyacheslav,
Thanks you for the quick response. Your solution works well!
Brian