2024-10-31 10:07 AM - last edited on 2024-10-31 10:25 AM by Andrew Neil
Hi,
I cannot connect to the NUCLEO-WB05KZ with the CubeProgrammer. Also tried the "Under Reset" option, I'm always getting the same error message:
" Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication"
How can I perform a discovery using Debug Authentication?
Solved! Go to Solution.
2024-10-31 10:21 AM - edited 2024-12-03 07:35 AM
Hello @Hen1
Coul you please try to connect this board using those parameters (and all other parameters combinations even debug in low power mode):
Also, Check the jumper positions: JP2 ON, JP1 on USB_STLK [1-2].
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-31 10:16 AM
Perhaps focus on the power and connectivity. So jumpers or solder-bridges.
2024-10-31 10:21 AM - edited 2024-12-03 07:35 AM
Hello @Hen1
Coul you please try to connect this board using those parameters (and all other parameters combinations even debug in low power mode):
Also, Check the jumper positions: JP2 ON, JP1 on USB_STLK [1-2].
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-11 04:40 PM - edited 2024-11-11 04:40 PM
Hi Guys,
thanks for your comments! All jumpers were at their right position, but I additionally connected the JP1 jumper on the MB2032 MCU RF Board. I dont know if that was necessary?
After some trying with different settings and unchecking "Debug in Low Power Mode", I could connect to the MCU.
It seems it's working now!
Best Regards,
Hen1