Enable BLE pairing of new devices on button press only
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-20 12:21 AM
As apart of the BLE capabilities in our project, which runs on STM32WB55
We want to allow pairing of new devices only when pressing a button.
When the button is not pressed, we want to allow connections of only devices which are already bonded.
From what I see that the SDK has no API for rejecting new pairing requests.
I also see that the HCI has an "authentication request command" which the SDK does not pass to the application layer.
The only two options I can think of are:
1. upon connection event (or "encryption changed event") disconnect the peer if it isn't in the bonding list.
2. The SDK does allow to manage a "white list" (which we can manage in parallel to the bonding list) and use it as a filter on the connection.
The white list is being managed on the RAM, which means we'll have to take care of its persistency on our own.
Am I missing something here? is there a better way to do it?
And isn't allowing only bonded devices a part of the core specifications?
Thank. Hagai
- Labels:
-
BLE
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-15 3:31 AM
Hello @hagaimoshe
You have nice ideas. Did you test this behavior. What I suggest you is to Just take a simple example and try to limit the number of connections to the number of devices already bonded and add more connections just when clicking on the button.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-07 12:15 PM
@hagaimoshe Did you find any solution for that problem?