cancel
Showing results for 
Search instead for 
Did you mean: 

Dynamic-concurrent mode Bluetooth Low Energy®/Zigbee in STM32WBA

justinjoseph
Associate

Hi Guys,
I was planning to start a project using the STM32WB55 chipset to implement a device capable of connecting to both Zigbee and BLE devices via a dynamic concurrent mode approach. I was able to confirm that this device supports it from the thread  https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_Dynamic_concurrent_mode_BLE-Zigbee I'd also like to confirm if the WBA series supports this feature. Given that the WB55 is a dual-core (M4/M0+), and the WBA series is based on the M33 core, I need to verify if the WBA series can support Bluetooth Low Energy® and Zigbee dynamic concurrent mode for this project. I couldn't find anywhere specific that says it doesn't support dynamic mode and I guess WBA is a very different series compared to WB. Please share your knowledge on this.

Looking forward for your response.

1 REPLY 1
STTwo-32
ST Employee

Hello @justinjoseph 

I can confirm that the Dynamic-concurrent mode Bluetooth Low Energy/Zigbee is supported by the STM32WBA. To understand how it works. You may can refer to this example: BLE_Zigbee/BLE_HeartRate_Zigbee.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.