2021-05-02 11:54 PM
Is it possible for stm32WB to recieve audio from a mobile device via bluetooth and at the same time send the audio to another device like headphones or wilreless earphones via bluetooth .Reception and Transmission should work simulteneously.Does it suppourt this ?
2021-05-03 11:30 AM
Many possible configurations with your question. Is it just a matter of transferring data packets containing audio samples from devices to another one with no data processing performed on STM32WB : No audio decoding/encoding performed on data sent/receive over BLE communications.
In that case, the device should just act as a simple router no matter the type of data it is transferring. this case is already supported. The point to carefully look at will be the bandwidth.
If some processing as to be performed, I am afraid the STM32WB does not nor support any official BLE codec such as the codec Low Complexity Communications Codec (LC3).