2019-07-30 10:33 PM
Hi Sir,
Like BlueNRG-2 have PCB antenna's of BLE232SA-A and BLE232UA-A Does STM32WB also have these kind of antenna modules???
2020-10-07 06:25 AM
No! The module is available internally but it needs some further tests and the ecosystem that helps developing a project with it is not ready yet.
2020-10-12 05:52 AM
Ok I am very glad for it because I have no complete RF knowledges, so I have a question, wich is one example of internal passive device? Is there an axample circuit with the use of internal passive device and a chip antenna?
2020-10-13 01:53 AM
What do you mean by "internal passive device"?
2020-10-14 04:33 AM
Hi sorry, I mean integrated passive device like is said in the document AN5165 on page 32, is there a preferred IPD with a mathced ceramic antenna? Or will be the release time of the STM32WB module not so long for us? :)
2020-11-26 01:52 AM
So, is the module live anytime soon ?
2020-11-27 06:50 AM
This product will be available very soon.
You can already order it: STM32WB5MMGHTR6
By week 01 of 2021, there will be stocks at distributors' sales points.
2020-11-30 01:56 AM
Is it possible to have the datasheet and the pinout to use it in a project under develpement?
2020-11-30 04:14 AM
Is it possible to have the datasheet and the pinout to use it in a project under develpement?
2020-11-30 05:45 AM
2020-11-30 06:01 AM
Thanks, I have see it is also available on the Cube. Can you please provide just the footprint so I can order the PCB while the component become avilable?