2023-11-23 05:56 AM
Hello,
I'm using the Nucleo-WL55CJ kit to test the Lora connectivity with TTN server.
At first, all worked fine and I received my data, but now the kit is unable to join the networt with the following error "DevNonce is too small".
Any idea?
Thanks.
Solved! Go to Solution.
2023-11-23 06:54 AM
Hello @laesser and welcome to the ST Community
The error message "DevNonce is too small" happens when using LoRaWAN MAC version 1.0.4 or 1.1, it's recommended to use LoRaWAN MAC version 1.0.2 or 1.0.1 (version 1.0.3 or lower) for your device.
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-23 06:54 AM
Hello @laesser and welcome to the ST Community
The error message "DevNonce is too small" happens when using LoRaWAN MAC version 1.0.4 or 1.1, it's recommended to use LoRaWAN MAC version 1.0.2 or 1.0.1 (version 1.0.3 or lower) for your device.
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.